ACTION#.ACTIVE
Description
Sets whether an action is disabled or enabled. When set to 1, the action will be executed if it is valid.
Value | Description |
---|---|
0 | Action disabled |
1 | Action enabled |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
ACTION1.ACTIVE |
3900h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION2.ACTIVE |
3900h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION3.ACTIVE |
3900h |
03h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION4.ACTIVE |
3900h |
04h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION5.ACTIVE |
3900h |
05h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION6.ACTIVE |
3900h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION7.ACTIVE |
3900h |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION8.ACTIVE |
3900h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION9.ACTIVE |
3900h |
09h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION10.ACTIVE |
3900h |
0ah |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION11.ACTIVE |
3900h |
0bh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION12.ACTIVE |
3900h |
0ch |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION13.ACTIVE |
3900h |
0dh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION14.ACTIVE |
3900h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION15.ACTIVE |
3900h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION16.ACTIVE |
3900h |
10h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION17.ACTIVE |
3900h |
11h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION18.ACTIVE |
3900h |
12h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION19.ACTIVE |
3900h |
13h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION20.ACTIVE |
3900h |
14h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION21.ACTIVE |
3900h |
15h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION22.ACTIVE |
3900h |
16h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION23.ACTIVE |
3900h |
17h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION24.ACTIVE |
3900h |
18h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION25.ACTIVE |
3900h |
19h |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION26.ACTIVE |
3900h |
1ah |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION27.ACTIVE |
3900h |
1bh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION28.ACTIVE |
3900h |
1ch |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION29.ACTIVE |
3900h |
1dh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION30.ACTIVE |
3900h |
1eh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION31.ACTIVE |
3900h |
1fh |
Unsigned8 |
- |
- |
Read/Write |
No |
ACTION32.ACTIVE |
3900h |
20h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
ACTION1.ACTIVE |
40100 |
9CA4 |
Unsigned8 |
Read/Write |
- |
ACTION2.ACTIVE |
40101 |
9CA5 |
Unsigned8 |
Read/Write |
- |
ACTION3.ACTIVE |
40102 |
9CA6 |
Unsigned8 |
Read/Write |
- |
ACTION4.ACTIVE |
40103 |
9CA7 |
Unsigned8 |
Read/Write |
- |
ACTION5.ACTIVE |
40104 |
9CA8 |
Unsigned8 |
Read/Write |
- |
ACTION6.ACTIVE |
40105 |
9CA9 |
Unsigned8 |
Read/Write |
- |
ACTION7.ACTIVE |
40106 |
9CAA |
Unsigned8 |
Read/Write |
- |
ACTION8.ACTIVE |
40107 |
9CAB |
Unsigned8 |
Read/Write |
- |
ACTION9.ACTIVE |
40108 |
9CAC |
Unsigned8 |
Read/Write |
- |
ACTION10.ACTIVE |
40109 |
9CAD |
Unsigned8 |
Read/Write |
- |
ACTION11.ACTIVE |
40110 |
9CAE |
Unsigned8 |
Read/Write |
- |
ACTION12.ACTIVE |
40111 |
9CAF |
Unsigned8 |
Read/Write |
- |
ACTION13.ACTIVE |
40112 |
9CB0 |
Unsigned8 |
Read/Write |
- |
ACTION14.ACTIVE |
40113 |
9CB1 |
Unsigned8 |
Read/Write |
- |
ACTION15.ACTIVE |
40114 |
9CB2 |
Unsigned8 |
Read/Write |
- |
ACTION16.ACTIVE |
40115 |
9CB3 |
Unsigned8 |
Read/Write |
- |
ACTION17.ACTIVE |
40116 |
9CB4 |
Unsigned8 |
Read/Write |
- |
ACTION18.ACTIVE |
40117 |
9CB5 |
Unsigned8 |
Read/Write |
- |
ACTION19.ACTIVE |
40118 |
9CB6 |
Unsigned8 |
Read/Write |
- |
ACTION20.ACTIVE |
40119 |
9CB7 |
Unsigned8 |
Read/Write |
- |
ACTION21.ACTIVE |
40120 |
9CB8 |
Unsigned8 |
Read/Write |
- |
ACTION22.ACTIVE |
40121 |
9CB9 |
Unsigned8 |
Read/Write |
- |
ACTION23.ACTIVE |
40122 |
9CBA |
Unsigned8 |
Read/Write |
- |
ACTION24.ACTIVE |
40123 |
9CBB |
Unsigned8 |
Read/Write |
- |
ACTION25.ACTIVE |
40124 |
9CBC |
Unsigned8 |
Read/Write |
- |
ACTION26.ACTIVE |
40125 |
9CBD |
Unsigned8 |
Read/Write |
- |
ACTION27.ACTIVE |
40126 |
9CBE |
Unsigned8 |
Read/Write |
- |
ACTION28.ACTIVE |
40127 |
9CBF |
Unsigned8 |
Read/Write |
- |
ACTION29.ACTIVE |
40128 |
9CC0 |
Unsigned8 |
Read/Write |
- |
ACTION30.ACTIVE |
40129 |
9CC1 |
Unsigned8 |
Read/Write |
- |
ACTION31.ACTIVE |
40130 |
9CC2 |
Unsigned8 |
Read/Write |
- |
ACTION32.ACTIVE |
40131 |
9CC3 |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
ACTION1.ACTIVE |
40100 |
Unsigned8 |
Read/Write |
- |
ACTION2.ACTIVE |
40101 |
Unsigned8 |
Read/Write |
- |
ACTION3.ACTIVE |
40102 |
Unsigned8 |
Read/Write |
- |
ACTION4.ACTIVE |
40103 |
Unsigned8 |
Read/Write |
- |
ACTION5.ACTIVE |
40104 |
Unsigned8 |
Read/Write |
- |
ACTION6.ACTIVE |
40105 |
Unsigned8 |
Read/Write |
- |
ACTION7.ACTIVE |
40106 |
Unsigned8 |
Read/Write |
- |
ACTION8.ACTIVE |
40107 |
Unsigned8 |
Read/Write |
- |
ACTION9.ACTIVE |
40108 |
Unsigned8 |
Read/Write |
- |
ACTION10.ACTIVE |
40109 |
Unsigned8 |
Read/Write |
- |
ACTION11.ACTIVE |
40110 |
Unsigned8 |
Read/Write |
- |
ACTION12.ACTIVE |
40111 |
Unsigned8 |
Read/Write |
- |
ACTION13.ACTIVE |
40112 |
Unsigned8 |
Read/Write |
- |
ACTION14.ACTIVE |
40113 |
Unsigned8 |
Read/Write |
- |
ACTION15.ACTIVE |
40114 |
Unsigned8 |
Read/Write |
- |
ACTION16.ACTIVE |
40115 |
Unsigned8 |
Read/Write |
- |
ACTION17.ACTIVE |
40116 |
Unsigned8 |
Read/Write |
- |
ACTION18.ACTIVE |
40117 |
Unsigned8 |
Read/Write |
- |
ACTION19.ACTIVE |
40118 |
Unsigned8 |
Read/Write |
- |
ACTION20.ACTIVE |
40119 |
Unsigned8 |
Read/Write |
- |
ACTION21.ACTIVE |
40120 |
Unsigned8 |
Read/Write |
- |
ACTION22.ACTIVE |
40121 |
Unsigned8 |
Read/Write |
- |
ACTION23.ACTIVE |
40122 |
Unsigned8 |
Read/Write |
- |
ACTION24.ACTIVE |
40123 |
Unsigned8 |
Read/Write |
- |
ACTION25.ACTIVE |
40124 |
Unsigned8 |
Read/Write |
- |
ACTION26.ACTIVE |
40125 |
Unsigned8 |
Read/Write |
- |
ACTION27.ACTIVE |
40126 |
Unsigned8 |
Read/Write |
- |
ACTION28.ACTIVE |
40127 |
Unsigned8 |
Read/Write |
- |
ACTION29.ACTIVE |
40128 |
Unsigned8 |
Read/Write |
- |
ACTION30.ACTIVE |
40129 |
Unsigned8 |
Read/Write |
- |
ACTION31.ACTIVE |
40130 |
Unsigned8 |
Read/Write |
- |
ACTION32.ACTIVE |
40131 |
Unsigned8 |
Read/Write |
- |